Other Parts Discussed in Thread: LDC2114
Hello!
What are the lighting conditions for the LEDs on the LDC2114EVM CPU board?
I think these are LEDs that indicate the target approach level (frequency increase level). What are the lighting conditions of the eight LEDs (D3-D10)? Is the level of DATAn (the largest DATA among DATA0 to DATA3) determined? If so, what is the discrimination level?
For example
LED1 DATAn> 256
LED1 & 2 DATAn> 512
LED1 & 2 & 3 DATAn> 768
LED1 & 2 & 3 & 4 DATAn> 1024
LED1 & 2 & 3 & 4 & 5 DATAn> 1280
LED1 & 2 & 3 & 4 & 5 & 6 DATAn> 1536
LED1 & 2 & 3 & 4 & 5 & 6 & 7 DATAn> 1792-
LED1 & 2 & 3 & 4 & 5 & 6 & 7 & 8 DATAn> 2048
Please provide correct information.
Best regards