Other Parts Discussed in Thread: AWR1642, UNIFLASH, AWR1642BOOST
Tool/software: Code Composer Studio
Hello:
According to the xWR16xx mmWave Demo, I encountered the following problems when running the AWR1642 BOOST:
1. In 4.3 Flashing CCS debug firmware, after opening Uniflash, which one should I select in New Configuration, AWR 1642 chip or EVM of AWR 1642 BOOST(see figure1)?
2. Also in this section, after filling in the port number, go back to the Program interface. The tutorial says that you need to restart the device and click Load Images again. Does it mean that I should turn on the board after power off? Besides, clicking on Load Images often results in loading failure (see figure 2,3), is that because the previous successful loading port is occupied, so it cannot reload after closing? If so, how can the occupied port be released? Or how to solve this problem?
Looking forward to reply!
Thanks!