AWR1642 short-radar design problem
My power and reset system is
Power and reset system with no power up sequence control
My problem is :
The AWR1642 can not work normally, it like that the AWR1642 not exit the reset state absolutely.
After power up , we use metal probe to click the TPS389033 reset pin, the AWR1642 can work normally!
My question:
- The power up sequence of AWR1642 has specific requirement or not ?
- The 3.3V supply is right or not;
I see the power up sequence of AWR1642 in the datasheet is