Hi,
What would be the max update rate that the 1642 would support? From the Demo visualizer, I'm seeing that it allows us to configure only upto 30fps. If this is true, what would be the suggestions to achieve an update rate of 100Hz?
On a related note, what would be the max velocity that the device can experience before which the range estimation will be accurate? Or in other words, if I just want to measure range, will residual Doppler be a problem?
I want to measure range and angle of arrival (if possible) for a high dynamics use case.
Thanks
Venkatesh