This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Dynamically Reconfigurable Configuration (CFAR, etc) Parameters

Part Number: AWR1843BOOST

Hi,

I'm wondering if the any of the configuration parameters that get sent to the board on startup (specifically the Range and Doppler CFAR parameters) are dynamically reconfigurable? Meaning that they could be re-written on the fly after startup via an mmWaveCLI service call?

Or does the board require a hard (disconnect/reconnect power) or software (using the 'sensorstop' CLI command + resending every CLI command in the config file) reset in order to change the Range and Doppler CFAR thresholds?

Thank you,

Carl