Part Number: TMP102EVM
Hi Sir,
the following picture is our use the TMP102EVM read All Reg function got waveform,
What is Area A Representative meaning?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hugo,
Region A is the master sending a Start condition, followed by a repeat of the address (0x48) and the read word bit. It is interpreted as: 100 1000 (0x48) + 1 (Read Bit).
Please see below, where I've enclosed region A on Figure 9 in the datasheet.
It can be helpful to think of each read operation that the GUI performs as a write operation (to the pointer register), followed by a read operation.
Best Regards,
Brandon Fisher