Other Parts Discussed in Thread: , DRV5055
We are using the DRV5033 in TO92 case hall sensor on a project, the problem is that each sensor switches at a different height from the magnet (within a 5mm difference). We have set up a jig so that the only variable is the hall sensor, we have the same voltage 3 volt, magnet is a Dia 4x8mm (+/- 83 Gauss) the magnet is 10mm away from the magnet. How do we get that all the sensors switch at the same height (within 0,3mm of each other)