This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVEICBOOST: IWR6843

Part Number: MMWAVEICBOOST
Other Parts Discussed in Thread: IWR6843ISK, DCA1000EVM,

Hi,

MMWAVEICBOOST cannot supply power, the drive cannot be installed, and the lights on IWR6843ISK are not on. The power adapter used is 5V, 3A, which can normally supply DCA1000EVM.The lights on the power adapter will also go off when you connect to MMWAVEICBOOST.Is there something wrong with my hardware?