This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP451-Q1: ALERT is turned off at startup.

Part Number: TMP451-Q1

Hi TI-team

My customer use TMP451-Q1.

ALERT output does not operate normally at startup.
After starting up, it once becomes High, but after about 200ms it becomes Low.
When customer read register (02h), it was d0. (BUSY, LHIGH, RHIGH flags are on)
 
Please tell me about the following two points.
1. What is the cause of the alert becoming L ?
2.What are the measures to keep ALERT going high after startup ?
 
Best Regards,
Koji Hayashi