This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: IWR6843

Part Number: IWR6843ISK


Hi sir,

I would like to know if that's possible to have mmWave to detect the surface of objects? Smooth or having gap on it.

Thanks for your help on this.

Best regards,

Janice

  • Hi Janice,

    Would you be able to clarify what you mean by the surface of objects? Is there a specific object or object material you are looking for?

    Cheers,

    Akash

  • Former Member
    0 Former Member in reply to Akash Gondalia

    Hello Janice,

    It may be possible to detect a gap in a surface thought it will depend on the material and dimensions of the gap. Typically this can be difficult to do with the standard point cloud demo in the out of box demo. It is likely the users would need additional post processing and algorithm work to identify the edges/corners where a gap occurs in the surface.

    Amanda