This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: requesting Support for editing firmware

Part Number: IWR1642BOOST

Tool/software: Code Composer Studio

Hi,

I want to know how to make a relay ON and OFF in the project containing inside the lab Area scanner for occupancy detection.I want to turn a Gpio on when an object is detected and turn  off when not detected .I am not able to find the function making a gpio as input and output  or turn on or off.Is that facility available in your board.I also want to detect the presence of an object having height 2.5m. if the height is more than 2.5m turn a gpio on else turn it off.

       Thank You.