Hello,
If an external reference were to be used to drive the DRV425-Q1's REFINT (pin 5) when the device is operated at 5 VDC, what is the max/typical input current that can be expected? It feeds the return leg of the DRV425-Q1's differential amplifier.
The data sheet doesn't specify this in section 6.5 under voltage reference or Shunt-sense Amplifier.
Thanks in advance.