Part Number: DRV5032
Hi Sir,
Would you pls kindly help customer's question about DRV5032? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ian,
This question, without any context, is unanswerable.
The customer will need to determine what type of magnet they wish to use to determine which BOP maximum threshold will be needed for their system.
Also, based on the use case/end equipment, they will need to determine if they want the device to be sensitive to either magnetic pole, or North/South only to determine if they need an omnipolar or unipolar style device.
I would recommend checking out this app note for some starter information on how to implement our switches. Do you have any details of a use case or end equipment that you can share? Just examining this device, the closest device I would recommend is the DRV5032FA, but I can provide a better recommendation with more information.