This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614-Q1: Conversion time

Part Number: LDC1614-Q1
Other Parts Discussed in Thread: LDC1614

Hi team,

I have a question about the conversion time for multi-channel operation mode of LDC1614 for 4channel.

CLKIN=40MHz

I would like to read out all 4 channel in 48msec cycle.

I set Rcount 25,000(0x61AB) which should be 10ms/channel and 40ms/4channel total conversion time to make sure <48ms of read cycle time.

But when I check the status register in 48ms, not all 4 channel is UNREADCONV.

Could you advise if there are any other register I should care about?

regards,

regards,