This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT70A: Engineers may find the following 4 quartic piecewise-polynomial for converting voltage to temperature

Part Number: LMT70A
Other Parts Discussed in Thread: LMT70, TMP117

The LMT70A  seems a very useful device, I am evaluating it as an IceCell 0C reference point replacement for themocouples.

Using the values in : 8.6 Electrical Characteristics Temperature Lookup Table (LUT)

engineers may find the following 4 quartic piecewise-polynomial for converting voltage to temperature :

It consists of 4 quartic polynomials (5 values each), constrained to be continuous in value and gradient at each breakpoint.
The last 2 columns are the breakpoints (voltages) for which each quartic is valid.

125.2532032081 -25.093326337 -0.2163930501 0.0980485104 -0.0323894142 302.785 574.06875
70.19241188 -29.9908860459 -0.17680832 -0.0080389126 -0.0053856012 574.06875 891.11625
15.1587296697 -24.9915729533 -0.1455544095 -0.007279563 -0.0007347763 891.11625 1149.00275
-32.3274977901 -22.4931203736 -0.1640761645 -0.0136061522 -0.0015646034 1149.00275 1375.219

At the quoted table temperature values the following graph shows the output temperature errors as a function of temperature :

So it seems to be better than 1 mK up to 100C. 

Using the table voltage for 0C of 1097.987, we get :

1097.987000      0.000079

Hope that this helps,

Dr. Beau Webber