Other Parts Discussed in Thread: AWR2243,
Hello,
I'm using four AWR1243Ps in cascade and having trouble with the phenomenon that the WARM_RESET PIN toggles repeatedly.
The MSS firmware on AWR1243P I'm using is included in MMWAVE DFP 01.02.05.01.
I have found the following in the Release Notes for MMWAVE DFP 02.01.05.03 for the AWR2243 and guess that this may be related to my problem.
3 Release Contents
3.2 Feature/Changes List by Components
3.2.2 Master SS firmware (DFP 2.0.3 – compared to DFP1.2/AWR1243)
Type:Bug
Key:MMWAVE_DFP-62
Summary:Fixed device is being resetting repeatedly due to Watchdog expiration.
Could you answer my questions below about this bug?
Q.1 Does this bug (MMWAVE_DFP-62) also occur in AWR1243P (MSS firmware of MMWAVE DFP 01.02.05.01)?
If the answer to Q.1 is yes:
Q.2 Is the WARM_RESET PIN toggling when "resetting" occurs in this bug?
Q.3 Please let me know the conditions under which this bug occurs.
Q.4 Please let me know if there is the workaround for this bug.
Thank you,
Sakamoto