Other Parts Discussed in Thread: PGA460-Q1,
hello everyone ,
i am looking for automotive ultrasonic sensor with LIN protocol compatible with hercules (TMS570lS1224).
detection range ( 10cm up to 3m).
is there any recommandations
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello everyone ,
i am looking for automotive ultrasonic sensor with LIN protocol compatible with hercules (TMS570lS1224).
detection range ( 10cm up to 3m).
is there any recommandations
AHMAD_OBAI,
The PGA460-Q1 supports a "LIN-like" interface called One-Wire UART. It is frame reduced and custom version of LIN specifically for the PGA460-Q1, and uses standard UART framework. If you are seeking a more traditional LIN interface, then the PGA450-Q1 is the only other option.
Both devices can support your 10cm to 3m range depending on the transducer used (recommending transformer driven at >=60kHz), though the PGA460-Q1 is our recommendation due to its improved performance and ease of use/programming.