Other Parts Discussed in Thread: TIDA-00151, PGA450Q1EVM, , TUSS4470, PGA460, PGA460PSM-EVM
Hello,
we are integrating a PGA450-Q1 on a custom board programmed with example program: PGA450-Q1_TIDA-00151_OTP-UART.hex. We are trying to sending command through serial 0x00,0x55,0x01,0x00 using TI-GER board following the instructions on sldu019b pag.7. No response from the sensor we also tried to send commands from a microcontroller at 5V logic levels 19200Baud rate. But no response from the PGA450. Using the PGA450Q1EVM GUI and putting the system in reset is it possible to read and write registers.
What are we missing?
Kind regards,
Matteo