This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2021: Asking for the design HDC2021 schematic and layout review

Part Number: HDC2021

Hi Team,

Customer is designing HDC2021 on the new project.

Would you please provide comment on schematic and layout review?

 

Here is schematic and layout file link.

You can use the free viewer.

 

BR,

SHH

  • Hi SHH,

    The schematic seems to be okay, but I'm having a bit of trouble seeing the schematic PNG as it appears to be very low resolution.

    For the layout, it looks like they have added several vias beneath the thermal pad of the device. The footprint recommended in the datasheet shows vias in the thermal pad as optional (see below). We typically recommend leaving these out. I would also make sure that they are using a split solder paste stencil like the one shown in this drawing. 

    Best Regards,
    Brandon Fisher