Other Parts Discussed in Thread: DRV421EVM
Table 2 in SLOU410A is incorrect. You can tell by examining the traces in Figure 5, or Figure 6, that the pin assignments shown in that table are not correct.
Additional comments:
-- Seems odd that the default value of R1 is 100 ohms. With a 5V supply, that limits the max field to 0.5 mT.
-- I much prefer the layout of the DRV421evm. Much easier to embed the evm, and make sensitivity tests.