This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV425EVM: Table 2 in SLOU410A is incorrect

Part Number: DRV425EVM
Other Parts Discussed in Thread: DRV421EVM

Table 2 in SLOU410A is incorrect.  You can tell by examining the traces in Figure 5, or Figure 6, that the pin assignments shown in that table are not correct.

Additional comments:

-- Seems odd that the default value of R1 is 100 ohms.  With a 5V supply, that limits the max field to 0.5 mT.

-- I much prefer the layout of the DRV421evm.  Much easier to embed the evm, and make sensitivity tests.