Part Number: BOOSTXL-PGA460
Other Parts Discussed in Thread: PGA460, , USB2ANY, MSP-EXP430F5529LP, PGA460-Q1, ENERGIA
Hi
I would like to evaluate the PGA460 for use in an ultrasonic indoor positioning system. In the end, there will be one mobile sender and multiple receivers, but for now evaluation of one sender and one receiver would be ok as well. Sender and receiver will be up to 5 meters apart, but never closer than about 0.5m.
Is there any way I can set this up with one or more PGA460 EVM? The struggle will be to synchronize both evalkits to the same time source. Even if there are cables which will limit the distance two EVMs can be apart, but is there a way at all to test this with the kits?