This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: +DCA 1000 EVM ::::: Use of USB and Ethernet extension cables

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: DCA1000EVM

Hi,

I am using a AWR1642BOOST + DCA1000 EVM. I am collecting raw 2x complex ADC data through these two EVMs and I am using mmwave Studio 2.0.0.2 also.

There was some problem of getting LVDS data from DCA 1000 EVM on Ethernet cable on my old laptop. Therefore, I bought a 100/1000 Gigabit Ethernet adapter (with USB hub). Now I have a newer laptop but I prefer to use USB hub with Gigabit Ethernet adapter for less hassle in the experimental setup.

I have plugged-in the following in the USB hub + Gigabit Ethernet adapter (2 in 1)

- One TI-provided USB cable from AWR1642BOOST EVM

- One USB cable from DCA1000 EVM (dont remeber if it came  with a USB cable or not ?

- One TI-provided ethernet cable from DCA1000 EVM

There is one single USB cable (15cm) output going from the above USB + Ethernet hub, into my laptop and things are working fine.

I wish to extend the length of this above USB cable from USB hub to my laptop. My questions are :

1)  Considering that I am already using a USB hub (with built in gigabit ethernet adapter) with 15cm USB cable, how much maximum length of additional USB extension cable I can use without (severely) effecting signal integrity ?

2)  What is the trade off on LVDS transfer rate of DCA1000EVM (maximum is 600Mbps) , when using the ethernet cable in a USB hub instead of directly using it in the ehternet (Rj-45) adapter of laptop ?

3) Is there a speed and / or signal integrity trade off if the two USB cables (one from AWR1642BOOST and one from DCA1000) are used as:

---  2 USB cables used in single USB slot of laptop through a USB hub

---- 2 USB cables used in a USB hub with builtin additional gigabit ethernet adapter

Thanks and regards