Hello,
In AWR2243 datasheet swrs223.pdf, Section 5.7 RF Specification, IF bandwidth is MAX 20 Mhz.
What is the MIN value of IF bandwidth? Does it depend on HPF1 setting as 175 KHz?
Thanks & Regards,
-Shibata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
In AWR2243 datasheet swrs223.pdf, Section 5.7 RF Specification, IF bandwidth is MAX 20 Mhz.
What is the MIN value of IF bandwidth? Does it depend on HPF1 setting as 175 KHz?
Thanks & Regards,
-Shibata
Hello Shibata,
I am not sure I fully understand. Do you mean what is the minimum configurable BW setting? You can configure the BW to be as low as 0 by setting the slope to 0 Mhz/usec.
Ingeneral users do not consider the objects seen within the HPF region, but that is the choice the user can make based on his application.
Regards,
Vivek
Hi Vivek,
Sorry for the confusion.
The IF bandwidth value found in the datasheet is only MAX value, 20 MHz.
I assume there are some variation depends on process variation or thermal drift.
If so, is it possible to share MIN value for IF bandwidth?
Regards,
-Shibata
Hello Shibata San,
Across process and temperature we guarantee that we can support 20Mhz IF bandwidth.
Regards,
Vivek