Other Parts Discussed in Thread: FDC1004
Hi,
I am currently evaluating FDC1004 using FDC1004QEVM for liquid level sensing. I have a few questions related to FDC1004 but before going to the questions, here is a little background of the application:
We are planning to use FDC1004 to estimate the water level inside the water tank of a hydroponics system. Because it is a hydroponics system, pH buffer and nutrient additive will be added to water regularly to ensure proper nutrient is being provided to the plants that are growing inside the system.
Questions:
1. If we were to use this in production, is there any recommended calibration procedures?
2.How do we calculate the gain and offset compensation value? Can we expect to use the same gain and offset compensation values for production or we will need to calculate these during calibration?
3. I suspect the property (dielectric constant) of water will change slightly when we add pH buffer and nutrient additive into the water tank. Do you think capacitive sensing is even suitable for our application? If not, do you have recommendation on other TI sensing products that are more suitable for our application?
4. I realized the Rigid-flex circuit doesn't come with the FDC1004QEVM kit. Is there a way we can purchase or get it from you for evaluation purposes?
Thanks,
Jeff