Other Parts Discussed in Thread: TIDEP-01021,
Tool/software: TI C/C++ Compiler
I read the Design Guide: TIDEP-01021.
In page:9 (2.3.2 Chirp Configuration and System Performance), it say Number of ADC samples is 256 and Number of chirps per profile is 256.
From what I test, AWR1843 with mmwave SDK 3.4.0.3 Demo can't set these two parameters to 256 at the same time.
1. Is there any way for me to use the parameters of Corner Radar on mmwave SDK Demo?
2. Do I need to make any modifications to mmwave SDK Demo in order to use the parameters?
Regards,
JuiYang