Hello experts,
I'm Namhyung and have some question about the AWR1642 ADC full scale and dBFS to dBm conversion.
I understand that the FS (full scale) is ADC's maximum power. Based on this and also many of your previous documents, the maximum ADC swing is +-1 V (2Vp-p) and the FS would be 10 dBm (0dBFS).
If we use 16 bit ADC raw data, +-2^15 code value would be +-1V, is this right?
This is my test result tested with mmWave studio. (the left FFT data is plotted without FFT window)
In this result, the averaged amplitude is around 11000 code and this would be around 33.5% of the full scale. It means that the value would be ~ -9.5dBFS.
But the mmWave studio shows around -13.5 dBFS and it shows about 4 dB difference.
Why this kind of difference happens?