Other Parts Discussed in Thread: USB2ANY, TUSS4470, MSP-EXP430F5529LP, UNIFLASH
I have new BOOSTXL-TUSS4470 and MSP-EXP430F5529LP evalutaion boards from TI and followed the setup instructions provided in the 'TUSS44x0 EVM for Ultrasonic Sensors User's Guide' (SLAU822A) section 2, 'Setup and Operation'. I have not made any changes to the hardware since receiving the boards and the jumpers have not been changed. The TUSS4470 is set to USB Only mode. After connecting the EXP430F5529 + TUSS4470 boards to the computer with the provided USB cable, the TUSS4xx0 EVM GUI version 1.0.0.6 displays 'Hardware Disconnected' and a Red circle in the bottom left hand corner of the window. I was able to run the MSP-EXP430F5529LP flash program as recommended by the TUSS4xx0 EVM GUI. After this, I tried the same steps in section 2 of the user's guide (SLAU822A) on another Windows 7 computer with the same results. I noticed in Windows 7 Device Manager (under 'Other Devices') on both computers, there is an alert/exclamation with a device labeled 'USB2ANY/OneDemo device'. The user's guide (SLAU822A) references USB2ANY in section 3, so I looked for drivers for this device on TI website but instead found the application USB2ANY explorer 2.8.2.0. I downloaded opened it. This is displayed:
ERROR No USB2ANY controller was found.
ERROR Open failed -Error -24: Invalid handle
Two green LEDs are lit up on each board, matching the appearance shown in the user's guide (SLAU822A) on page 5, Figure 3. I did try two separate USB cables on two different computers. Both computers are using .NET versions above 4.5 : 4.8 and 4.61. I tried to install .NET 4.5 but It failed with the message, "Same or higher version of .NET Framework 4.5 has already been installed on this computer". I tried each cable with multiple ports on each computer, but the EVM GUI is unchanged, reporting "Hardware Disconnected" and Device Manager shows the same alert as before (USB2ANY/OneDemo). Is there anyone on this forum with the same issue? Thanks,
John