Other Parts Discussed in Thread: TLA2022
When using a 'scope to probe the LMT70's output, the voltage drops somewhat. We can determine this because we have an ADC (TLA2022) and firmware reporting the output.
The probe is 10 Meg, 13 pF, and yet the drop is about 100 mV out of, say, 800 mV. We're also seeing the output drift slowly over time, on the order of 10 C or more in either direction, in a quiescent system without significant changes in the room temperature.
Is there any reasonable explanation for this, or do we have damaged ICs? Are they unusually sensitive to handling or soldering?
Thanks,
Scott