This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: XA1243FPBGABL

Part Number: AWR1243


HI,

I'm working with two XA1243FPBGABL chip connected in cascade configuration.

I have a problem during the boot of the system, i try to program the chip master in Functional SPI mode but the SPI_HOST_INTR signal after going on high level after the power on, remains always high.

The path of the MOSI is correct in according with the SPI_CLK and SPI_CS.

the control signal that i used, connected to the host,  are : SPI_CS, SPI_CLK, MOSI_1, MISO_1, SPI_HOST_INTR_1, NRESET, NERROR_OUT

The SOP configuration is : SOP2=0, SOP1=0, SOP0=1

I wanted to know what could be the cause of the problem (SPI_HOST_INTR signal remains high) and if the control signals used are correct or if someone is missing for the configuration in Functional SPI mode.

Thanks

Best Regards