Hello
We purchased one of your LDC1614.
We had a large iron-core coil has an inductance of ~1.4H.....when we get it close to a piece of metal this inductance reaches 1.9H. This experiment failed, while using a PCB spiral coil managed to give more useful results.
Questions;
- Do we have to use spiral coil with your LDC or can we use any coil?
- Is there a limit on the inductance we can measure using LDC1614?
- We understand that this LDC can detect a change of frequency of ~0,2Hz. We understand also that there is a range for the resonance frequencies that this LDC can work with and hence we choose the correct capacitor. Do you have any explanation for the lack of success (apart from the iron-core coil and large inductance, if they were a reason).
Regards
Sam