This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP464: how to mask D4 over temperature warning output through THERM pin

Part Number: TMP464

hi Team,

my customer uses TMP464 channel D1/3/4 for measuring remote temperature but they only want THERM pin report the over temperature warning on channel D1/3 and the warning of D4 needed to be ignored.

so how can we achieve this requirements?

Can we set 30h bit11 to 0 to disable the conversion on Channel 4? will this mask D4 over temperature warning through THERM pin?

or should they set the thermal limit to a high value so that the over temperature will never be triggered?

thanks.