Other Parts Discussed in Thread: AWR1642, AWR1843BOOST, AWR1843,
Hello everyone,
I have a question regarding the "Obstacle Detection" example lab coming with Automotive Toolbox. I have noticed that, TI AWR1642 was only able to detect a target and do dBscan clustering up to 3m.
Even though, the default profileCfg shows 10m as a maximum detectable range. Here is the default chirp config:
sensorStop flushCfg dfeDataOutputMode 1 channelCfg 15 3 0 adcCfg 2 1 adcbufCfg -1 0 0 1 1 profileCfg 0 77 7 7 58.0 0 0 67.978 1 256 5020 0 0 36 chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 2 frameCfg 0 1 32 0 100 1 0 lowPower 0 1 guiMonitor 1 1 0 0 cfarCfg 1 4 12 4 2 8 2 200 30 2 0 5 20 dbscanCfg 4 4 13 20 3 256 sensorStart
Even I am lowering the CFAR threshold from 350 to 150, I wasn't able to detect anything above around 3m.
In dbscanCfg command, the second number is related to the "Max distance allowed in clustering (in units of 0.1m), depending on the object size". Is that mean dBscan algorithm will only do clustering if individual detections are seperated each other max. 0.4m?
Can you please guide me how to re-configure the TI AWR1642 so that I would be able to get a detection and clustering output above 3m?
Thank you for your help
Aybars Kizilay