Other Parts Discussed in Thread: UNIFLASH, AWR1642
Tool/software: Code Composer Studio
Dear reader,
I am trying to implement the short range radar code and driver vital signs from resource explorer in ccs.
I downloaded the PC GUI for both cases.
In the first one the GUI comes up but nothing happens, in the notes there is something about binarys, downloading them and flashing them on the radar. Where are these files located? And is that why it isn't working?Moreover does this show the usage of 80m and 20m together?
In the second case when i try to play the program i get the missing Qt5Gui.dll error. I tried puting the file in the same directory as the program and in system but it didn't work. How can i fix this?
Also are the codes the one used in the program or something else?
Kind regards,
Nilo