my customer want to know if we have the P2P solution with ALPS HGDEDM013A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Scott.
For an in-plane device we have recently released TMAG5123 that is p2p and will also sense the magnetic field along the length of the package.
hi Arjun,
thanks for help. but seems HGDEDM013A has 4 pinout here, and our TMAG5123 just have 3 pinout.
not p2p here.
do we have p2p solution or if we have the very close solution here?
Weijin,
TMAG5123 is currently only offered in the 3 pin SOT23 package.
DRV5032DU is a four pin, dual output version with somewhat similar thresholds, but will still maintain the z-axis of sensitivity. It is offered in the X2SON package, which is close in size to the MAP package of HGDEDM013A, but doesn't appear to be quite the same physical dimensions.
Thanks,
Scott