Hello,
I am using LMT86LPGM for monitoring the ambient air temperature. I am facing a weird problem i.e when I turn on my PCB, I could see the temperature measured is quiet correct(about 27 degrees). But after some time the value shoots to very high like 150 degrees. This is happening with multiple sensors. I also checked the voltage on the output of the sensor and it shows 1.8V at the beginning of the test and suddenly starts to decrease to a very low value like 500mV. I am not able to find the root cause. Below is the temperature profile from one of the tests. Also attached is the schematics. I tried different values of series resistance on the sensor output line like 2.2K, 3K, 4.7K, but the problem persists.
My sensor is mounted on a different PCB and that is connected to my MCU using Flex. Also, for proper mounting I have cut short the leads by 7mm . Can that cause this problem?
Kindly help with the possible root cause analysis and fixation to the problem.
Thanks,
Siddharth