Hi Team,
I have a question about TMP275 I2C communication.
TMP275 datasheet figure 9 shows Two-Wire Timing Diagram for Read word format.
When we see end of transfer(byte2 bit9), that SDA is ACK.
However, when we see NXP I2C bus specification, there is comment that "5.A master-receiver must signal the end of the transfer to the slave transmitter.".
Question here is should we send NACK at byte 2/ bit9 or send ACK as datasheet figure 9?
refer to https://www.nxp.com/docs/en/user-guide/UM10204.pdf
Regards,
Kai