Other Parts Discussed in Thread: LMP91000
Hi
we are designing a voltammetry circuit using LMP91002, we tried [8.1.2 Sensor Test Procedure] providing VDD=3.3V, DGND=MENB=AGND=GND, 10K resistor is connected between C1 & C2, An electrode is connected as per the requirements CE WE RE are connected, we got Vre = 1.689V, Vwe=1.651V, but unable to measure Vrw , & VOUT = 1.651V, we are getting a stable voltage of VOUT = 1.651V even when the electrode is dipped in the solution, we are unable to check the change in voltage
Thanks & Regards
Sasikumar E