Hello, There are several questions need to confirm:
1, Per the OPT3006, there are 16 black rectangle blocks on the bottom side, if the sensor function independently, considering the SMT alignment , if only 2~4 blocks exposed. if the function will be ok?
2,We need to dispense underill glue to waterproof the sensor, as the pad is so close to the cutout edge, there will be glue overflow to the slot area, the underfill will influent the function, What is the minimum size of exposured area except for the overflow? Is transparent underill glue works if we dispense the whole cutout area? Or do you have any recommend method?
3, Is there any inspection standard regarding to the foreign partical in the cutout area of the sensor?
Appreciate for your reply. Thanks you very much!