Hi community member,
I saw mmwave IC's datasheets (IWR1443, IWR1843, IWR6443, IWR6843).
According to these datasheet, the each ramp rate is as below:
- IWR1443, IWR1843(77GHz) : Max 100MHz/us
- IWR6443, IWR6843(60GHz) : Max 250MHz/us
Is it the reason that IWR6xxx(60GHz) is newer devices than IWR1xxx?
I'm interested in why is the difference.
Best regards.
Cruijff