This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: TMP112/TMP116

Part Number: TMP112
Other Parts Discussed in Thread: TMP116, TMP117EVM,

Hi,

I'm a college student doing a Project on infrared temperature. I was given TMP007EVM but unfortunately, it was outdated. The support engineer requested me to buy TMP112 or TMP116 to replace it. I have bought the components but how do i incorporate it inside TMP007EVM.

This what the customer chat told me. "For your query , Normally if we had he schematic , we can find the device place and pin arrangement, we can guide you to welding of the old device and replace the new one . But for your query, the TMP007 is obsolete, we had to delete all the information about it, I can not make sure that TMP116 or TMP112 can replace the TMP007 directly"

Please retify this problem,Thank you 

  • Dear S Gokula Krishna - 

    Welcome to E2E and thanks for posting!

    Neither the TMP116 nor the TMP112 are infrared temperature sensors, I can confirm that for you.

    If your project is about that specific type of sensing, as the TMP007 is discontinued and we are not making IR temp sensor at this time - then I need to ask here if you just need the User's Manual and GUI to use the EVM or it is broken in some way? We don't have any more in stock, but there are a few in the distribution stock I can see from searching the web.

    or is your project about temperature sensing in general, where, we could suggest the TMP117EVM or the TMP112EVM?

  • Dear Josh Wyatt

    My school project is to produce a wearable infra-red thermometer. But right now I have TMP 116 and TMP 112 along with TMP007. Is there a way I could buy any components and create a PCB board and built the infrared thermometer?

    thank you 

  • Dear S Gokula Krishna -

    The TMP007 is discontinued. The TMP116 and TMP112 are not infrared temperature sensors, so I think this is a blocked path with these components as choices.

    Is the TMP007EVM broken in some way or do you just need the User's Manual and GUI to use the EVM, without modification?

  • Dear Josh Wyatt,

    Are we able to buy any infrared temperature sensors to modify the TMP007EVM?

    Yes please, I would also like to have the  User's manual and Gui to use the EVM

    Thank You 

  • just sent you email - closing this post