This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ultrasonic sensor distance range from 50mm to 1000mm

Other Parts Discussed in Thread: PGA450-Q1, PGA460, MSP-EXP430F5529LP, MSP430F5529

I am currently working on an application that requires an ultrasonic sensor to determine the ice level in an ice making machine.

I need to be able to read levels from 50mm to 1000mm.  I have looked into using the PGA450-Q1, but  the application note has a distance range from 7 meters to under 1 meter.  Will it go as low as 50mm?

There is one other issue that concerns me.  I see that the PGA450 has an integrated 8051, but how much code would I be writing on the 8051 for an application such as mine?  In my case I will have a processor in the design and would much rather have all my code there instead of maintaining two separate ones.

What would you recommend in my case?

  • Hi Jairo,

    Since the PGA460 has numerous enhancements compared to the PGA450, I would recommend the PGA460 here. The PGA460 supports multiple communication interfaces, which can be used to configure the device using an external microcontroller. The BOOSTXL-PGA460 EVM specifically shows the use of the PGA460 with the MSP430F5529 microcontroller that is in the MSP-EXP430f5529LP Launchpad board.

    In regards to your question on distance, Section 2.8 of SLAA907C provides more details on how to improve the minimum detection range.

    Regards,

    Mekre