Other Parts Discussed in Thread: TIDA-00317,
I am currently using the TIDA-00317 reference design along with the FDC1004QEVM board.
I experienced a situation where the liquid levels would take approximately 5 minutes to drop to the correct level when water was removed from the beaker. However, when the beaker would fill up the levels would display correctly in a matter of seconds. The problem was constant until I removed the sensor board along with the double sided tape and laid it out flat on the table. After not bein able to reproduce the problem I went ahead and folded the sensor tail along with the board and reattached it. I have not been able to reproduce the problem since then. Any ideas as to what may have caused the problem? I have the sensor attached to a 1000ml plastic beaker. I've attached a photo of my setup.