Other Parts Discussed in Thread: DXP
Hi Team,
My customer considers using TMP431 with not using remote sensor.
How to connect DXP and DXN in this case?
The datasheet shows two contents about it which is correct? Are both contents OK?
----------------------------------------------------
(datasheet page 14)
When not using the remote sensor with the TMP43x, the DXP and DXN inputs must be connected together to prevent meaningless fault warnings.
(datasheet page 33)
Tie the DXP pin to GND if the remote channel is not used and only the local temperature is measured.
----------------------------------------------------
My customer will set "(Configuration register 2) REN bit =0" in this case.
Best Regards,
Yaita