Other Parts Discussed in Thread: LDC1314, LDC1612, LDC1614
Excuse me.
I adjusted each register so that the voltage of the INA0 pin would be about 1.5 (V).
However, even if an aluminum target is placed on the LC sensor, the value of the [RCOUNT0] register changes only about 400 to 430.
I want to increase the range of change in the value of the [RCOUNT0] register under the condition that the value of the [OUTPUT_GAIN] field of the [RESET_DEV] register remains 0b00.
Please give me some hints.
By the way, each parameter is as follows.
The value of C is 1000 (pF).
The value of L simulated by [Coil Designer] is 7.89 (uH).
The Resonance impedance displayed in the Coil Designer is 1822.4 (Ω).
The logic of the [HIGH_CURRENT_DRV] field in the [CONFIG] register is 0b1.
The value of the [DRIVE_CURRENT0] register is 0xD800.
Please.