Other Parts Discussed in Thread: TMP108, TMP144
Hello team,
I received a question about temperature error of TMP103.
Can you answer the following question?
Looking at the TMP103 data sheet, the resolution is 1 °C,
Ambient temperature is -10 ℃ to 100 ℃, the maximum error is stated as ± 2 ℃.
Ambient temperature of -40 ° C to 125 ° C, the maximum error is stated as ± 3 °C.
■ Question
- Does the error in the output value increase as the ambient temperature becomes strict?
- Is it possible to reduce the error by calibrating the initial value?
Best regards,
Shotaro