This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: Failure in Time (FIT) Data

Part Number: TMP112

I am interested in Failure in Time (FIT) data for the part number TMP112AIDRLT. Specifically I was hoping to get:
1. The temperature at which the FIT testing was done
2. The FIT E9 value (after 1 billion hours) or the FIT E6 value (after 1 million hours)
3. The activation energy (Ea) of the chip

  • Ranger,

    The FIT data available to provide for the TMP112 is below. Keep in mind this is for the TMP112AQDRLRQ1 orderable. (TMP112-Q1)

    Component Failure Rates per IEC TR 62380 / ISO 26262 Part 11

    • Total FIT Rate- 4
    • Die FIT Rate- 2
    • Package FIT Rate- 2

     

    Component Failure Rates per Siemens Norm SN 29500-2

    • Category- CMOS/BICMOS ASICs Analog and Mixed ≤ 50-V Supply
    • Referenced FIT Rate- 25 FIT
    • Reference Virtual- 55°C

    Jalen