This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004QEVM: How to adjust the GAIN value to bigger?

Part Number: FDC1004QEVM
Other Parts Discussed in Thread: FDC1004

Hi,

I use FDC1004QEVM with Sensing Solutions EVM GUI V1.10.0 to test liquid level.

Because my container is only 35 mm, the level changes is little.

I set the GAIN value to 3, and the value is 1.943 pF to 2.564 pF (from empty to full level).

If I want to see the bigger delta, does it have any method to set the GAIN over 3?

Thanks