Other Parts Discussed in Thread: HDC2022
hi:
Hdc2010 is used in IPx4 waterproof structure.
Because it is waterproof, it exists in closed space.
The air enters into the structure through waterproof and breathable membrane (IP54 standard) to detect the temperature and humidity.
From the current test data, the temperature can reach the ambient temperature after one hour, which meets the accuracy requirements.
But after one hour, the humidity can not reach the ambient humidity.
Question:
1. In your understanding of customers, based on the requirement of waterproof grade, do you have temperature and humidity?
2. If so, under normal temperature, the humidity is normal, and it can be stable in a few hours?
3. Can you provide information on the application of temperature and humidity in waterproof products (such as cases, precautions, design avoidance, etc.)