Other Parts Discussed in Thread: AWR1642BOOST, AWR1642
Hello Champs,
Can the C:\ti\mmwave_automotive_toolbox_2_9_1\labs\lab0001-driver-vital-signs demo run on AWR1642BOOST-ODS board?
Thanks.
Rgds
Shine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Champs,
Can the C:\ti\mmwave_automotive_toolbox_2_9_1\labs\lab0001-driver-vital-signs demo run on AWR1642BOOST-ODS board?
Thanks.
Rgds
Shine
Hi Shine,
The developer's guide and release notes for the lab only specify the AWR1642BOOST EVM to be compatible, so I doubt the lab would ever have been tested for ODS. Still, I will forward this question to the rest of the team and get back to you.
Regards,
Aayush
Hi Shine,
[EDIT]: The following statement is incomplete.
I have just confirmed this with my team, the vital signs lab is not supported on AWR1642 ODS.
[EDIT]: Apparently the vital signs lab only uses 1TX and 1RX, so the difference in antenna pattern in the ODS EVM is irrelevant. It should be possible to run the lab on ODS. I am not sure if this has ever been tested though.
Regards,
Aayush
Hi Aayush,
Thanks for your reply.
Customer failed to run the vital sign lab on AWR1642BOOST-ODS, he followed the Getting Started Guide and clicked the Start button in VitalSignsRadar_Demo.exe, then there is no output.
So I am not sure if the vital signs demo doesn't support AWR1642BOOST-ODS board or the customer didn't follow the steps correctly.
Below is the log:
QT version = 5.9.1
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "COM7"
User Port Number is "COM8"
Data port succesfully Open
User port succesfully Open
QWindowsWindow::setGeometry: Unable to set geometry 1485x999+8+31 on QWidgetWindow/'MainWindowWindow'. Resulting geometry: 1370x749+8+31 (frame: 8, 31, 8, 8, custom margin: 0, 0, 0, 0, minimum size: 1347x749, maximum size: 16777215x16777215).
Configuration File Name Read from the GUI is %s/n "xwr1642_profile_VitalSigns_20fps_Back.cfg"
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
"COM8"
Configuration File Path is %s/n "D:/Program Files/ti/ccs930/mmwave_automotive_toolbox_2_9_1/labs/lab0001-driver-vital-signs/vitalSigns_host/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg"
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 1"
"guiMonitor 0 0 0 0 1"
"calibDcRangeSig -1 0 0 0 0"
"vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
"motionDetection 1 20 2.0 0"
"sensorStart"
""
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 1"
"guiMonitor 0 0 0 0 1"
"calibDcRangeSig -1 0 0 0 0"
"vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
0.3
0.9
4
"motionDetection 1 20 2.0 0"
"sensorStart"
""
Chirp Duration in us is : 50
Chirp Bandwidth in kHz is : 3500
Maximum Range in Meters is : 8.57143
Range-FFT size is : 256
Range-Bin size is : 0.0334821
Range-Bin Start Index is : 8
Range-Bin End Index is : 26
Total Payload size from the UART is : 260
Padding Factor is : 9
Total Payload size from the UART is : 288
Thanks.
Rgds
Shine